Other Parts Discussed in Thread: LM5175
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5175 工具/软件:WEBENCH设计工具
我们为 LM5175上的12v 8A 降压/升压设计了该板、
但电路板不支持超过4A 的电流(仅47瓦的功率),
当我们将负载增加到4A 以上时,输出电压 Vout 从12V 降至9V。
请提前向我们推荐解决此问题的方法
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.