Other Parts Discussed in Thread: LM337
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM337 您好!
我需要-42V 和-20V 之间的可调电压。
例如、在|VI-VO|< 40V 的情况下、我能否将 LM337负极 LDO 用于-45V 输入?
或者、在任何情况下-37V 是较低的输出电压?
提前感谢、
此致、
斯特法内
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.