请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5116 你(们)好
我的客户设计了一个电源模块, Vin 为48~60V,输出 为 12V@4A,满负载效率为89%。 但在空载模式下,待机功耗约为2.5W,太高,我们找不到原因,您能不能提供帮助?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.