请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28881 一些 逻辑器件的客户设计辅助电源、输入电压为270V 至15V/0.02A。
问题在于、启动后、Vout 跳转到60V 并持续200ms、然后向下跳转到原理图下方的15V.see
你可以帮帮我吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.