请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28180 当我的客户使用 L4891A 时、输出电压可达到2.2 μ F 的小纹波。
ucc28180是否可以使用相同的输出电容器来实现更小的输出纹波?(输入电压:18VAC~40VAC、输出电压:60V、120W)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.