请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS50601A-SP 在计算并联操作的补偿值(C1、C2和 R3)时、数据表中的状态是使用单个设计的计算结果、然后并联设计将是系数2。 这是否意味着我应该将单个计算值乘以2来计算新的并行值? 如果我有4个并联的器件该怎么办?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在计算并联操作的补偿值(C1、C2和 R3)时、数据表中的状态是使用单个设计的计算结果、然后并联设计将是系数2。 这是否意味着我应该将单个计算值乘以2来计算新的并行值? 如果我有4个并联的器件该怎么办?