请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM34936大家好、
我们是否有任何降压/升压解决方案可替代 ADI LTC3119?
客户需求:
·在升压模式下:Vout (max)=18V、Iout = 2A
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.