Other Parts Discussed in Thread: UCC28911
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28911 您好!
UCC28911 EVM 原始设计用于5V 输出。 是否可以稍微重新设计(调整一些电阻器)以实现15V 输出?
谢谢!
-落基山脉
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.