Other Parts Discussed in Thread: DCR010505
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DCR010505 大家好、
我的客户电路板上没有3V 电源轨、他们是否可以为 DCR010505中的 SYNC 引脚使用3.3V?
我发现数据表建议同步3V、如下所示:
建议施加到 SYNC 引脚的最大电压为3V
请帮您就此提供一些建议吗?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.