请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ2000EVM 对于3节镍氢电池、我将 J5设置为374k 电阻器、并使用6伏电源为电路供电。
充电似乎在每节电池大约1V 时切断、电池大部分是空的。
我需要使用6伏的电压为该芯片供电、 我希望使电池组电压高达4.2伏。 我是否需要对 bq2000evm 模块执行其他操作才能使其正常工作?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.