Other Parts Discussed in Thread: LM43603
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM43603 您好、先生、
LM43603的反馈电压在轻负载时不稳定(约60mA)
测试结果:
输出电压18~20V:引脚9 FB 电压= 1.011V
输出电压3~17V: 引脚9 FB 电压= 1.024V
请帮您检查,非常感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.