Other Parts Discussed in Thread: TPS568215
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS568215 大家好、
我发现 TPS568215存在异常现象。
测试条件输入12VDC 转换器输出 5VDC。
验证 EVM 在输出侧额外增加了电源电压5.5V、输入电压将升至30V 直流。 为什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.