Other Parts Discussed in Thread: TPS53317
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS53317 您好!
我推出了一款需要高电流 VTT 以用于 DDR4存储器终端的新设计。 我发现 TI 具有 TPS53317 @6A、但我需要具有更高电流(8A)的 TPS53317。 非常感谢您能为该问题提供任何解决方案! 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.