Other Parts Discussed in Thread: TPS61196
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61196 您好!
我们使用 TI BU 中的直流调光电路、我们发现当使用模拟调光将 LED 电流调整到9mA 以下时、TPS61196无法进行分流。 (TPS61196故障引脚将不高)
是否有任何想法、我是否希望通过模拟调光将调光电流降至0mA。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.