请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS54308 我有一个使用此降压稳压器生成5VDC 的应用。 I -可能-偶尔会出现输入电压降至5VDC 的情况。 由于数据表声称此器件可以具有100%的占空比、我想知道这是否意味着直通模式、我可以摆脱5VDC 输入。
谢谢!
Jerry Wasinger
Pi-Plates.com
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.