Other Parts Discussed in Thread: TPS25200
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS25200你好。
我正在寻找一个包含单个5V 输入和两个稳压输出的组件。
一个限制为5V @1.5A、另一个限制为5V@0.5A。
您能否提供合适的解决方案?
Gilad。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.