Other Parts Discussed in Thread: TPS3808
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS3808 如果 TPS3808上的 CT 引脚连接到1/2电源轨(在 Vdd = 3.3V 的情况下为1.65V)、器件是否会将其解释为被拉至 Vdd、然后提供300ms 的延迟?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.