请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS84259 您好 BU 朋友、
您可以帮助查看 TPS84259的原理图吗?
VIN 为12V、Vout=-5V;客户告诉我输出仅为-0.794V、而不是-5V。
感谢您的帮助。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.