请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM73606-Q1 您好!
您能否帮助分享 LM73606-Q1的热测试结果?
输入:12V
输出:5V/6A@500kHz、5V/6A@2.1MHz、3.3V/6A@500kHz、 3.3V/6A@2.1MHz
环境温度:25°C、85°C。
谢谢。
东宝
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
您能否帮助分享 LM73606-Q1的热测试结果?
输入:12V
输出:5V/6A@500kHz、5V/6A@2.1MHz、3.3V/6A@500kHz、 3.3V/6A@2.1MHz
环境温度:25°C、85°C。
谢谢。
东宝