主题中讨论的其他器件:LMZM33604、 LMZM33606、
您好!
我需要一个稳压器、该稳压器将从正5伏产生负5伏电压。 建议使用额定电流超过2A 的开关稳压器。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、Vishwajit、
回答您在11月5日提出的两个问题
按照先前链接的应用手册、在反相拓扑中使用 LMZM33606器件、以在2.2A 下实现5Vin 至-5Vout。 数学计算使用较差的预期效率(70%)、如下所示:
2. LMZ34002没有任何用于电流共享功能的专用 SH 引脚。 因此、LMZ34002的配置方式无法与 您的5Vin 至-5Vout @ 2 - 2.2A 应用共享大于效率图中所示最大0.6A 的电流。
此致、
Jimmy