请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS2660、 TPS2663我想使用 efuse (TPS2660)作为330W 的电源、为56V 和6A、这是可行的吗? 如何连接组件以实现正确的功能? TPS2660是2.23A 的n´t 选择、但我想测量6A、我认为并联三个电流是可以的、但我不知道是否可能。
感谢您的支持!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.