尊敬的 TI:
TPS55340 输入=12V 输出电压=24V、输出电流=500mA 输出电流=90%+。
但是、当进行浪涌测试时、输入电流超过限制 ILIM。 原理图和波形显示为 foldw:
电流限制:
关断:输入电流波形:超过5.8A
我在 Cin 附近添加了470pF、导通波形会更好、但关断波形不变。
我想知道如何提高性能,非常感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.