Other Parts Discussed in Thread: TPS7A92, LP5922
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP5922 主题中讨论的其他器件:TPS7A92、
对于 LP 5922的输出上升波形、我希望 CNR / SS = 0nF 时的数据。
对于其他条件、请将条件 VIN = 1.7V、VOUT = 0.9V 或接近该条件。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.