请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:BQ76930、 BQ76940我们希望开发越野电机的电池 BMS。
平均电流为30A、但峰值电流为200A (最后3~5秒)。
也就是说、当 放电电流为200A (最后3~5秒)时、需要确保 D_FET 导通。
此外、所需的电池节数为13s。
哪种 AFE 满足此类要求?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.