Other Parts Discussed in Thread: TPS7A45
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS7A45 大家好、我的 TPS7A45设计如下所示。
但是、当引脚1为低电平以禁用 TPS7A45时、输出大约为-0.5V。 我还尝试在引脚4上放置500欧姆以提供负载、但没有做任何改进。
如何在 TPS7A45被禁用时防止负输出?
谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.