Other Parts Discussed in Thread: LM3150
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM3150 你(们)好
建议将 LM3150的 Cboot 设置为0.33uF 至0.47uF。
1。
如果电容值大于建议值、对运行有什么影响?
2.
如果电容值小于建议值、对运行有什么影响?
贝斯特雷加兹
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.