Other Parts Discussed in Thread: BQ25895
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25895 您好!
我的客户正在使用 BQ25895、因为放电电流可能高达9A。
充电电流仅需2A@5V。
下面的原理图是否正常? 尤其是 D+ D-。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.