Other Parts Discussed in Thread: TPS65177
大家好、
SWBK1的波形非常奇怪、当开关关闭时、电压大约为2V。
Robin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、辽卡特、
Vin=12V、VIO=3.3V。 这用于 TCON IO、VIO 将为 Vcore = 1.8V 供电、SWBK1用于 VGL1。 负载不会在较大范围内变化。
我使用 RT6914进行测试、它非常稳定。
最奇怪的是、当开关关闭时、SWBK1的低电平大约为2V。 发生这种情况的原因是什么? 如果有人建议挖掘根本原因,我可以同时从当地的角度去做。 客户不能等太久。 TPS65177可被许多引脚2引脚竞争产品所取代。
Robin