Other Parts Discussed in Thread: BQ25120
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25120 我们有一个低功耗应用、锂离子电池和辅助电源的充电电流为2-2mA。 BQ25120具有很大的前景、因为它具有内部直流/直流转换器、因此可提供高效率。 但是、数据表中提到它仅适用于5mA 充电电流。 是否有办法将此 IC 配置为2-3mA 充电电流?
提前感谢
DS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.