Other Parts Discussed in Thread: TPS54040
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS54040海
我是一名设计人员、正在为我的设计寻找低噪声电源。我需要两种不同的降压稳压器、分别用于3.3和5V 电源。两者的电流供应能力需要在500mA 或更低的范围内。请分享您有关这方面的建议。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.