请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM317 我尝试使用具有12 VDC 输入和3.3VDC 稳压电压的 LM317。 规格中用于维持稳定(VI−VO = 40V)的最小负载电流为 最小电流提供"-"、典型值和最大值提供3.5mA 和10mA。
负载可以小于1mA、也可以高达~ 20mA
如果我将 A 负载电阻器与负载并联的大小设置为825欧姆、我可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.