Other Parts Discussed in Thread: TPS61258
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61258 尊敬的 TI 专家:
我的客户检查 了1个 TPS61258样片的标记、发现 YMS 为"221"。 您能帮您建议如何对其进行解码吗? "22"是指哪一年和哪一个月? "1"表示哪家组装工厂? 规则如何工作? 非常感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.