请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:BQ2060A、 BQ25703A我们需要支持4.2V、4A+、4节电池、NTC 和 I2C 的锂离子电池充电器。
我们计划使用来自正常壁式扭曲适配器的12V (65W+)。
您是否有任何部件支持这些要求?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.