请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC256302 你好。
我对 UCC 256302的 OCP 3阈值有疑问。
数据表中显示了 OCP 3阈值的变化
℃℃̊ C 至125 ̊ C:0.49V 至0.79V。
-10℃至125℃的变化是如何的?
℃、25 ̊ C 环境温度下的变化是多少?
典型值:0.64V = 25°C 是否正常? 是否存在变体?
谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.