Other Parts Discussed in Thread: LT1054
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LT1054 您好!
我想使用 LT1054、我有两个问题:
-我想从15V 输入或5V 输入生成-15V 电压、但我读出最大电压为15V。 它在15V 电压下仍然正常工作吗?
-我想提供高于100mA 的电流,我能否将两个器件并联,同步它们?
谢谢、
Jacopo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.