Other Parts Discussed in Thread: LM25085
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM25085 您好、先生、
我们正在为 12V~26V 至12V/5A 应用寻找 LM25085 100%占空比解决方案。
但 TI WEBENCH 显示"计算出的占空比超过限制"。
LM25085是适合此应用的解决方案吗? 还是任何建议 的同步降压?
Hugo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.