请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ34Z100 主题中讨论的其他器件: BQ40Z80
大家好、
目前,我必须设计一个电池供电设备,其中电池功能为7.4V,电池容量为10Ah,电池节数为6。
当我浏览 BQ34Z100电量监测计的数据表时,没有关于电池节数的说明,该 IC 是否可以与我的电池一起使用(包含6节电池),请提出建议?
此致、
Karthik
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.