尊敬的先生:
我们的客户参考 PMP6013来设计具有 TRIAC 调光控制 LED 驱动器的 AC90~130输入电压和直流21~39输出电压。 它可以打开8S LED 板,但 当我们调整 TRIAC (LUTRON CT-603PG)时,它会有一些点动,您有没有建议我们 微调 TRIAC?
最恰当的考虑
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的先生:
感谢您的回复。 由于我们从客户那里获得了此原理图,我可以将其发送到您的电子邮件吗? 我们尝试了2种 LED 板,分别为11s/10P 和8S/9P,然后11/S/10P 可以通过 TRIAC 正常调光控制,波形如图1图片2 (图片1是全开,图片2是全关), 但8S/9P 有一些像图片3和图片4 (图片3是全开的,图片4是转向滑动的),我们如何微调电路?BTW, 下面是我们变压器的规格,供参考~
通道1 = Vout
通道2 = Iout
通道3=VCC
通道4 =交流电流
L1 (主) : 58 圈 @ 0.25mm
L2 (二次): 33转@ 0.25mm
L3 (Aux) : 25 转@ 0.25mm
L1: 580uH
此致
Jason