Other Parts Discussed in Thread: UCC28780
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28780 使用 UCC28780D、封装16引脚 SOIC、启动时请勿工作、此时 HVG 为5.1V、SWS 为6.2V、VDD 为5.1V、REF 为0V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HVG、SWS 引脚和耗尽模式 MOSFET 没问题、VDD 引脚无法达到17.5V、这可能是由什么引起的? 电路图为 :www.ti.com.cn/.../tidrux1.pdf