请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5176 大家好、
我的客户有以下要求:输入电压为13v~56V、输出电压为12v 5A、频率为500kHz;无论我们是否可以使用 LM5176来实现该要求、一个问题是器件的最大输入电压仅为55V。 一个问题是、最大占空比可能不够。 谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.