请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS62148 根据数据表、TPS62148可提供12VDC 的最大输出电压。
我可以在芯片上使用的最低电源电压(VIN)是多少、但仍然可以获得12 VDC 输出?
我在12 VDC 下的最大电流消耗将为400mA。
谢谢、
Matt
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.