请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ76940 主题中讨论的其他器件:BQ76930
当外部平衡打开:Ω 时、bq76930电池电压似乎上拉
绿色曲线是电池电压-最小(电池电压)(mV)、
当蓝色曲线上的点= 50时、表示该电池上的平衡处于打开状态。
采样周期= 1000ms。
为什么会这样呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.