请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM2621 主题中讨论的其他器件:TPS61088
我想将3.7V-5V 输入转换为10V 输出。 我准备了一个电路,但没有得到10V。 输出电压为
4.88v 而不是10V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.