Other Parts Discussed in Thread: TPS549A20
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS549A20 大家好、
我的客户希望将 TPS549A20 PMBus 地址设置为0x26 (8位)。
我检查了数据表、可以使用255k + 27k Ω 进行设置、对吧?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.