请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS54620我使用5V 输入、通过 TPS54620输出1.8V、电流3A、 HDMI 输出、波形和其他参数、这些参数是正常的。μ A
当我使用9V 输入时、HDMI 输出将会产生噪声、原因是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.