Other Parts Discussed in Thread: LMZ23605
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMZ23605 大家好、
数据表规定了典型的软启动时间为1.6ms。 您能告诉我该值是如何测量的、即10%到90%或20%到80%吗?
谢谢、此致、
Felix
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.