Other Parts Discussed in Thread: LM5119
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM5119您好!
对于 TI 的非隔离式直流/直流控制器、是否有人认为达到以下规格是一个好主意?
VIN=12V 至48V
VOUT=7.2至9V
Iout=>100A
谢谢
开始
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.