Other Parts Discussed in Thread: BQ24210
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:BQ24210我们需要锂离子电池充电器 IC、电池容量为2600mAh 3.9 V、
IC 要求
输入电压范围为5至10 VDC 太阳能电池板
我们需要状态指示
输出充电能力为500mA 和1A
建议我 哪种 IC 适用?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.