请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS543C20 主题中讨论的其他器件:TPS543B20、
尊敬的 E2E:
由于 总输出电流低于65A、TPS543C20是否可以与 TPS543B20堆叠?
如果是、在总负载电流高于50A 的情况下如何处理电流共享?
BR、
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.