请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM2623、 LM3481、 TPS61221主席女士,
是否有输入电压范围为0.5V-5.5V、输出电压为3.3V、输出电流为0.5A 的直流/直流转换器?
请提供建议。 谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.